跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How I can know the version of the device file?

Latest Updated:12/01/2011

Question:

How I can know the version of the device file?

Answer:

Version information can be displayed using the device file installer (DFINST) included with 32-bit version development tools.
For a device file already installed, version information should be displayed in the lower window of DFINST.

If the device file is not installed yet, select the folder containing the device file whose version information you want to display using the [Browse] button in the upper window.
The device file information in the selected folder is displayed.