跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Functions of EEPROM Pack for RL78 MCUs access control to dfl?

Latest Updated:04/04/2014

Question:

Which functions of the EEPROM Emulation Library Pack 01 for the RL78 family of MCUs operate the access control to data flash memory (DFLEN)?

Answer:

Executing the EEL_Open and EEL_Close functions respectively permit (DFLEN=1) and prohibit (DFLEN=0) the access to the data flash memory.
Suitable Products
Flash Self Programming Libraries
Data Flash Libraries