跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

E0562011 Invalid parameter specified in option "input" : "***.obj"

Latest Updated:09/18/2015

Question:

The following error message is output during building.

E0562011 Invalid parameter specified in option "input" : "***.obj"

Answer:

This message indicates the –input option has been specified for a filename or pathname which includes parentheses.

Parentheses used in a filename or pathname are interpreted as parentheses enclosing a sub-option, since the format for "libraries (modules)" supports the designation of modules within libraries for the –input option.

Change the filename or pathname to one without parentheses.

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family