跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Does the software for PG-FP5 flash programmer included upon purchase?

Latest Updated:11/21/2014

Question:

If I buy the PG-FP5 flash programmer, does it come with the software required to use it?

Answer:

The PG-FP5 does not include the required software (listed below). Get the software from the Renesas Electronics website.

  • Programming GUI (including the USB driver)
  • Parameter files (PR5 files) for the PG-FP5*
    *The parameter files differ according to the device you are using.

Web page: http://www.renesas.com/pg_fp5.
Click on the [Downloads] tab on the above web page.

Suitable Products
PG-FP5