跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Do I use a ROMization processor in V850 FlashROM SRAM environment?

Latest Updated:12/01/2011

Question:

In a V850 + FlashROM + SRAM environment, all the executable programs of the system are written into flash memory.
In this case, do I have to use the ROMization processor?

Answer:

If you use a configuration in which a variable with an initial value is used or a program is executed in RAM, you have to use the ROMization processor.
Suitable Products