跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Characters are garbled in CSV file read by Smart Configurator for RZ

Last Updated:08/02/2017

Question:

If a CSV file output by the Smart Configurator for RZ is read by Excel, the characters in the file are garbled.

Answer:

The problem occurs because CSV files that can be output by the Smart Configurator for RZ V1.10 are coded in UTF-8.
To display the file correctly, use the following procedure.

1. Open the Memo Pad, and then drag the output CSV file to the Memo Pad.
2. Make sure that the data is displayed correctly in the Memo Pad, and then save the file as is.
3. When you open the CSV file overwritten by Excel, data in the file is displayed correctly.
Suitable Products
SC(Smart Configurator)
Code Generator