跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can you tell me the applicable scope of a patch option -patch=7055?

Latest Updated:09/10/2007

Question:

Can you tell me the applicable scope of a patch option -patch=7055?

Answer:

This is a patch option to circumvent a SH7055-specific bug. Since a SH7058-specific bug has already been fixed, you do not need to use this for SH7058. When you use this option, it generates source code for workaround. It affects on size and performance of your source code, but does not cause any illegal operation.
Suitable Products
C/C++ Compiler Package for SuperH Family