跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can connected E8 emulators be used from the flash development tool kit?

Latest Updated:07/25/2008

Question:

[Flash Development Tool Kit V.3, V.4]: When multiple E8 emulators are connected to one PC, can each E8 emulator be used from the flash development tool kit?

Answer:

The Flash Development Tool Kit cannot be used when multiple E8 emulators are connected to one PC.
The Tool Kit cannot identify each E8 emulator and therefore may connect to an emulator other than the one you want to use.
Suitable Products