Bus width cannot be set to 16-bit or 32-bit in RX Code Generator Plug-in
Last Updated:08/02/2017
Question:
How can I set bus width to 16-bit or 32-bit in the RX Code Generator Plug-in or AP4 for RX?
Answer:
To specify 16-bit or 32-bit bus width, select the BC1/WR1 pin check box. For details, refer to "16.4.1 Data Alignment Control for CS Area" in the user's manual for hardware.
Example: When selecting the CS1 bus width in RX71M buses
Suitable Products
e² studio |
CS+ (formerly CubeSuite+) |
Code Generator |