跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Are those lines displayed on window of IO Wizard represents output?

Latest Updated:09/04/2009

Question:

Are those program lines displayed on status window of IO Wizard during peripheral settings representing the program lines generated on the output .c file ?

Answer:

Yes, all program lines displayed on status window will be generated on the output ,c file. However, the order of program lines shown in status window and program lines generated on the output .c file might not be the same.
Suitable Products
 
  • 本文是否實用?