跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

ANSI/ISO Specifications: "Standard Template Library" supports ?

Latest Updated:09/10/2007

Question:

User's manual says that the compiler is compliant with ANSI/ISO specifications. Is the STL "Standard Template Library" supported ?

Answer:

No. Our compiler does not support the STL "Standard Template Library".
Suitable Products
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for H8SX, H8S, H8 Family