跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

"Where is CPU information file? "

Latest Updated:09/10/2007

Question:

Where is the CPU information file which is one of the [Verify options] of linkage editor?

Answer:

The CPU information file was supported in the previous versions of compiler.

(Previous version compiler generated the CPU information file

to check the consistency of allocated address for section,

but the latest version compiler checks the consistency without the CPU information file.) F

or the latest version compiler, just specify an address area with a verify option. If a section which is actually assigned to program exceeds the area specified by [Verify option] , an error message is displayed on the output screen when executing a build.

Suitable Products
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for H8SX, H8S, H8 Family