跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What do files with the filename extension .mrc contain?

Latest Updated:06/12/2015

Question:

What do files with the filename extension .mrc contain?

Answer:

Files output with the filename extension .mrc were output by CC-RX and contain lists of service calls that are used in C source files. They were for reference in linking service calls to the kernel libraries for the RI600V4 and RI600PX. However, RI600V4 V1.04.00 and later versions have been changed so that they do not require reference to .mrc files.
Suitable Products
RI600V4 Real-time OS for RX Family
RI600PX Real-time OS for RX Family