跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Unable to Create New Project for RI600V4

Last Updated:02/21/2018

Question:

CS+ does not recognize installation of RI600V4, and I cannot create a new project for RI600V4. How do I resolve this?

Answer:

In the CS+ menu, select [Tool] >> [Plug-in Setting...], and then check whether the check box for the following plug-in in the [Additional Function] tab has been selected.

    Plug-in for real-time OS build setting (Common)

Then, select the check boxes for the following plug-ins.

    Plug-in for task analyzer tool (Common)
    Plug-in for real-time OS resource information display (Common)
    Plug-in for real-time OS analysis setting (Common)
 

Suitable Products

RI600V4
  • 本文是否實用?