跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How do I handle frequent interrupts with the RI600V4 without causing problems?

Last Updated:05/17/2017

Question:

Has the RI600V4 been designed with an algorithm that can handle frequent interrupts? I know that an interrupt that requires a significant amount of time to be handled is unable to be implemented. Is there an index to handle this?

Answer:

In theory, the RI600V4 has been designed to handle frequent interrupts. However, in practice, they may delay a task operation or consume CPU power, and the task may not run at all. To avoid this, we recommend avoiding frequent interrupts and interrupts requiring a lot of time for processing.
Suitable Products
RI600V4
  • 本文是否實用?