跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Differences between Evaluation Edition and Trial Edition

Last Updated:02/21/2018

Question:

There appears to be three versions in Real-time OS: evaluation edition, product version, and trial edition. What is the difference between the evaluation edition and the trial edition?

Answer:

The evaluation edition is a license for development of trial products.
There is no restriction on quantity to embed the Real-time OS, but the evaluation edition is only available for development of trial products.

The trial edition has restrictions compared to the product version and evaluation edition, and allows you to easily evaluate product features and productivity. However, note that no support (including responses to inquiries) is provided for the trial edition.
 

Suitable Products

RI600V4
RI78V4 V2
RI850V4 V2
RX Family
RL78 Family
  • 本文是否實用?