跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Wiring connection between MCU and E8 or E8a

Last Updated:10/18/2017

Question:

What is the correct wiring connection between the MCU and E8 or E8a?

Answer:

Refer to the E8/E8a Users manual published for the target MCU for wiring details. User Manuals are available at the following sites:

E8 Document Site
E8a Document Site

Suitable Products

E8
E8a
  • 本文是否實用?