跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Why there's error dialog when I download program to internal Flash ROM?

Latest Updated:07/17/2008

Question:

The following error dialog pops up when I download a program to the internal Flash ROM using the E10A-USB emulator for SH MCUs and click GO (execute program), even though I haven't exceeded the guaranteed number of rewrites for the internal Flash ROM.

       Error: "Flash memory write error! Change device"

Answer:

This error occurs when a write (or erase) event to the internal Flash ROM fails. The cause of the error is most likely one of the following.

  1. The "system clock" or "clock" value input when the E10A-USB emulator was started was incorrect.

    SH7047F, SH7144F or SH7145F: input the "system clock" value.
    The "system clock" value is the CPU operating frequency. For example, if a 10MHz clock is input and the CPU is run at 4 times the clock speed, the "system clock" should be 40MHz.

    For all other MCUs: input the "clock" value that was input to the MCU.
     
  2. The state of the FWP pin (hardware protect pin for internal flash memory write/erase) is incorrect.

    SH7047F: Make sure the FWP pin is set to low.
    All other MCUs: FWP and FWE (hardware enable pin for internal flash memory write/erase) can be set to either high or low.
     
  3. The settings of pins MD0 and MD1 are incorrect.

    SH7047F, SH7144F or SH7145F: Set A and B as shown in the table below.
      MD1 MD0
    A 1 0
    B 1 1
Suitable Products
E10A-USB