跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

List of know-how when using E1/E20 emulator in CS+ environment

Last Updated:04/26/2017

Question:

List of know-how when using the E1/E20 emulator in the CS+ environment

Answer:

Helpful information for using the E1/E20 emulator in the CS+ environment is listed below.
If you are facing any trouble, the FAQ portal sites for troubleshooting or error message are available.

Category Suitable MCU Description FAQ NO.
Target board Design/
Connections
RX About wiring connection during debugging via the FINE connection. 1010672
Could pins to which trace facilities are assigned be used as pins for facilities other than tracing? 1011183
V850 Could the port pin be used through CSI connection even though the port pin isn't shown as a HS pin in the user's manual for the device? 1011176
RL78 About reset lines 1011179
About the pull-up resistance value of the TOOL0 pin 1011180
Programming Functions RX How to read out the content written into the internal flash memory. 1010762
How to download programs and data to the flash memory connected to the external bus of the RX microcontroller. 1010501
V850 How to download programs and data to the flash memory connected to the external bus of the V850 microcontroller. 1011177
Debugging Function All MCUs How to stop the program execution when a specified address was accessed. 1010571
How to start debugging from the startup routine 1010513
RX, V850, RH850 How to debug the pin functions whose user port is multiplexed with the microcontroller pins 1010239
How to use the RAM monitoring facility (to view contents of memory while a program is running) 1011220
RX Difference from running the program on the user system as a stand-alone unit 1011217
Advanced Usages V850, RL78, 78K How to output objects in the binary format 1010510
Precautions/
Restrictions
RL78

How to set the on-chip debug option byte for a program to be used in mass-production

1010547
Suitable Products
CS+ (formerly CubeSuite+)
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]