跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is there a connector for converting the FoUSB 10 pins to the E8a 14-pins?

Latest Updated:07/24/2008

Question:

Due to discontinuation of the M3A-0065 FoUSB, it was recommended that I switch to E8a. Is there a connector for converting the FoUSB 10-pins to the E8a 14-pins?

Answer:

Yes. Please use the conversion connector E8 14PIN-10PIN Convert Board (R0KZC000000002R).

This connector was developed to support the M16C Family, which uses a 7-wire connection. Please note that this connector does not, however, support the R8/Tiny Series.
For details concerning the conversion connector, click here.
Suitable Products
E8a