跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is an area reserved in H8S/2329EF can be also used in E10A-USB?

Latest Updated:03/12/2008

Question:

E10A-USB can be used with H8S/2329EF even in the ROMless mode. However, the space from address H'060000 to H'080000 in Area 0 is a reserved area in H8S/2329EF.
Can this area also be used with E10A-USB?

Answer:

No. The areas that can be emulated by E10A-USB are the same as those shown in the memory map in the MCU hardware manual.
Suitable Products
E10A-USB