Information about RX family MCUs with E1/E20 emulator and the HEW
Latest Updated:04/26/2017
Question:
It is my first time to develop an application using RX family MCUs with E1/E20 emulator and the High-performance Embedded Workshop.
Can you tell me which documents will help me? Are there any information as references?
Can you tell me which documents will help me? Are there any information as references?
Answer:
Refer to the following.
Name of References | References | Reference Sections | Descriptions | ||
---|---|---|---|---|---|
Basic Operations | E1/E20 Emulator Additional Document for User's Manual | E1 | E20 | Section 3 Preparations for Debugging Section 6 Tutorial | From activation the High-performance Embedded Workshop to basic debugging operations with the E1/E20 emulator. The tutorial program is designed to help users to understand how to use the functions of the emulator and emulator debugger. |
E1 On-Chip Debugging Emulator Application Note Introductory Guide for the RX610 Group | E1 | 3. Installation 4. Let's Try Using the E1 Emulator | This introductory guide is intended for first-time users of the E1 emulator and provides simple instructions. | ||
Debugger Functions | E1/E20 Emulator Additional Document for User's Manual | E1 | E20 | Section 5 Emulator Functions | The emulator functions the E1/E20 emulator supports |
High-performance Embedded Workshop User's Manual | E1/E20 | 17. Debugging Facility | Common functions of emulator products operated under the High-performance Embedded Workshop. | ||
[Emulator Help] in the High-performance Embedded Workshop [Help] menu | - | - | The E1/E20 emulator functions + The emulator functions on RX family MCUs. | ||
[Help Topic] in the High-performance Embedded Workshop [Help] menu | - | - | Common functions of emulator products operated under the High-performance Embedded Workshop. | ||
Troubleshootings | E1/E20 Emulator User's Manual | E1 | E20 | 3. Troubleshooting (Action in Case of an Error) | How to solve a trouble when any problem occurs before the emulator debugger starts after the emulator and the user system have been powered on. |
E1/E20 Emulator Additional Document for User's Manual | E1 | E20 | Section 7 Notes on Usage | Restrictions on using the E1/E20 emulator | |
On-Chip Debugging Emulator E1/E20 Troubleshooting Guide (for the RX600 Series) | E1 | E20 | 1. Troubleshooting on Startup 2. Troubleshooting in Operations after Startup | This document gives examples of problems and remedies for these problems for user debugging with RX600-series MCUs. | |
FAQ | E1 | E20 | - | The faq page for E1/E20 emulator | |
FAQ List of troubleshootings | E1/E20 | - | The FAQ portal site of the common question when using the E1/E20 emulator | ||
FAQ List of error messages | E1/E20 | - | The FAQ portal site of the error message that E1/E20 emulator outputs | ||
Fault | E1/E20 Emulator User's Manual | E1 | E20 | Appendix A Self-Checking Program (SCP) | The procedure for using the self-checking program for the E1 and E20 in fault analysis. |
Latest Information | Tool News | E1 | E20 | - | Information about the upgraded versions, the precautions and etc. |
Etc. | External Flash Definition Editor User's Manual | E1 | E20 | - | Introductory guide for the utility software "External Flash Definition Editor" that create the definition files to write to an external flash memory by GUI operations easily. |
External Flash Definition Editor Application Note Creating a Custom Program | E1 | E20 | - | A summary of the procedure for creating a custom program that is specifiable in the External Flash Definition Editor | |
FAQ List of know-how | E1/E20 | - | The FAQ portal site which know-how on using the E1/E20 emulator is summarized |
Suitable Products
E1 [R0E000010KCE00] |
E20 [R0E000200KCT00] |