跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Error message-Not enough memory_E10A-USB

Last Updated:09/27/2017

Question:

I am using E10A-USB (HS0005KCU01H or HS0005KCU02H) for H8S,H8SX. When I download a program, I get the following error message. How can I avoid this problem?
Error message: Not enough memory

Answer:

This error message is displayed when the target memory for the downloading cannot be accessed for some reason. Check the following as possible causes.

Does the selected download address include a reserved area of the target MCU?
Does the selected download address exceed the address space of the target MCU (in other words, does it include an area higher than address H'1000000)?

Suitable Products

HS0005KCU01H
HS0005KCU02H