Error message: downloading program to 78Ko in E1 or E20 from CubeSuite+
Latest Updated:10/24/2014
Question:
When I downloaded a program to the 78K0 family microcontroller through the E1 or E20 from CubeSuite+, the following error message appeared.
Error (E0210002)
Launching debugger failed.
[Direct Cause of the Error]
Illegal condition. (E1201024)
Answer:
Set [Main clock source] as "Generate by emulator".
Suitable Products
CS+ (formerly CubeSuite+) |
E1 [R0E000010KCE00] |
E20 [R0E000200KCT00] |