跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Current consumption with CS+ and E1 debugging circuit_RL78

Last Updated:12/13/2017

Question:

In E1/E20/E2 Emulator, E2 Emulator Lite Additional Document for User’s Manual (Notes on Connection of RL78), it is stated that “the on-chip debugging circuit in the device operates during on-chip debugging. Therefore current consumption of the device increases.”
How much will current consumption of the device increase with the debugging circuit in the device?

Answer:

We do not have our own specifications for current consumption. When evaluating current consumption of the device, do not connect the E1 /E20 /E2 Lite.
E1/E20/E2 Emulator, E2 Emulator Lite Additional Document for User’s Manual (Notes on Connection of RL78)
Suitable Products
E2 Emulator Lite [RTE0T0002LKCE00000R]
E1 [R0E000010KCE00]
CS+ (formerly CubeSuite+)
  • 本文是否實用?