跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Could the programmer be used through CSI connection?

Latest Updated:09/22/2014

Question:

I am using the E1 (or E20) emulator for the V850 family.
Could the programmer be used through CSI connection in this case even though there is no description of the HS pin in the user's manual for the device?

Answer:

Since HS is the name of a pin for use by the programmer, it may not be described as a multiplexed pin in the user's manual for the device.
In this case, connect the port pin to which the HS pin function has been assigned (for example, the HS pin function is a multiplexed function of the PCM0 pin in the V850ES/JJ2).
For the corresponding port pin, see the description on communications with the programmer (CSIB0 + HS, CSIB3 + HS) in the user's manual for the device.
Suitable Products
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]