跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Collection of Error message_E8a_E8

Last Updated:11/15/2017

Question:

The error message appears, and the E8a/E8 is not operated correctly.

Answer:

Refer to the following FAQs.

Note: The limitations of E8a/E8 differ depending on the MCU used in your systems. Please confirm each item of [Notes on Using the E8a Emulator] on the [E8a/E8 Emulator Additional Document for User's Manual] to find a solution for your case.
You can download [E8a Emulator Additional Document for User's Manual] from here .

Timing of 
occurrence
Suitable
Emulator
Suitable MCU Error Message FAQ No:
starting-up/
connecting
E8a/E8 All “FDT will now update the E8/E8a firmware to a newer version to allow connection to the device (current Adaptor Software (Level x) version = x.xx.xx.xxx, new version = x.xx.xx.xxx) Click OK to continue” 1000323
"Boot Failed""Communication Timeout Error""Target missing" "Cannot find device driver or connection was cancelled" 107346
“Target device driver missing, or connection cancelled.” 1000235
E8a "Driver Error: No available communication devices found. Unable to set default configuration for Renesas E-Series USB Driver" 1000053
Toolchain *****, version ***** is missing from the following project(s) ***** ”There is no compatible toolchain. Build functionality will not be available.” 1000238
R32C/100 Group "Failed to identify the firmware ID code." 1009868
debugging E8a All 
(except H8 family)
"There is no response from MCU. Recover the state by resetting MCU?" 1000141
E8a/E8 M16C, M32C 
family
"Communication Timeout Error" 106856
M16C/62P,
M16C/6N Group
107058
M16C/60 Series 106960
All 102357
H8 family "Stack Pointer in guarded area" 1000058
"Programcounter is odd""Stack pointer is odd" 1000059
All "Not available now." 107557
"Memory area error. It overlaps the system range." 106672
"Memory area error. It is outside the effective address range" 1000068
"Invalid address value" 106394
"ILLEGAL INSTRUCTION" 107352
"Too many parameters" 107490
programming/
downloading
E8a/E8 H8 family "program size is exceeds Flash memory size" 107348
M16C family "ID code error" 106426
All "Communication Timeout Error" 107032
"Can not use RESET function" 106971
R32C/100 Group "not enough memory" 1000060
E8a All "Error erasing flash memory" 1000065
H8 family "ID code error" 106964
 
  • 本文是否實用?