跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can these E8a, E8, E10A-USB and E10T-USB emulators be used in 1 PC?

Latest Updated:03/31/2009

Question:

Concerning use of emulators E8a, E8, E10A-USB and E10T-USB, can several emulators (either several of the same type or a combination of types), be used on one PC ?

Answer:

Yes.
However, when using more than one emulator at the same time, you will need to run one High-performance Embedded Workshop for each emulator.
When more than one of the above emulators is connected to the same PC at the same time, the channel or serial number* for each emulator will appear in the Driver details dialog when the PC is turned on.

* Display message:
E10A-USB/E10T-USB/E8: channel
E8a: serial number
To switch emulators, select the corresponding channel or serial number. (refer to figure below)

Suitable Products
E10A-USB
E8a
E10T-USB
E8