跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Different type of compiler under a floating license

Last Updated:05/17/2017

Question:

Is managing a different type of compiler under a floating license possible? For example, is it possible to manage licenses for both the Standard edition of CC-RH and the Professional edition of CC-RX at the same time?

Answer:

Yes, managing licenses in this way is possible.
 
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 本文是否實用?