跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Requirement for Using Annual License

Last Updated:11/29/2017

Question:

I am considering purchasing an annual license.

Do I need to purchase a permanent license to use the annual license?

Answer:

No, you do not.
Since the annual license and permanent license are independent licenses, you can use the annual license without the permanent license.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 本文是否實用?