跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Inhibiting output of the .option byte section (CC-RL)

Last Updated:05/10/2017

Question:

I am using the CC-RL compiler for RL78 devices. An option byte section (.option_byte) has been generated without my intending this. I want to specify non-output of this section in the output files (.abs and .mot). Can I do this? I am trying to divide the memory area of the MCU into two parts, and to create output files individually.

Answer:

You cannot inhibit the generation of .option_byte in abs files.

Generate the file as .mot, then specify output of the ranges of addresses or sections in the mot file that exclude .option_byte.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • 本文是否實用?