跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

One Year Validity of Annual License Means

Last Updated:11/29/2017

Question:

It is written that annual licenses are valid for one year. Does this mean I can use the license for one year on the basis of actual compilation time?

Answer:

No. It will expire on the date after one year from initial registration with the Renesas Web site of the code for obtaining the license which accompanies the compiler product.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 本文是否實用?