跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Installing a Floating Compiler License key on a PC with a Node Locked License installed

Latest Updated:12/14/2016

Question:

Can I install a Floating Compiler License on a PC which already has a Node Locked License installed?

Answer:

Yes, if you have a compiler under an Node Locked License on your PC, you can use both that and the Floating License environment once you have installed the software for the PC to work as a client for the Floating License product.

(Examples) 
Node Locked License environment: CC-RL 
Floating License environment: CC-RX 
or 
Node Locked License environment: CC-RX 
Floating License environment: CC-RX

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 本文是否實用?