跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to restore section name to default? (CC-RL)

Last Updated:06/21/2017

Question:

I am using the RL78 CC-RL compiler.

I have changed a section name using #pragma section to allocate a variable in an arbitrary section.
Is there any way to restore the variable section defined after that to a default section name?

[example]

#pragma section bss MyBss
int __near ni_1;        //MyBss_n Allocated a variable in a section
int __near ni_2;        //Want to restore the variable to the section

Answer:

Section names can be restored to default if a section type and new section name are not specified and #pragma section is specified instead.

[example]

#pragma section bss MyBss
int __near ni_1;        //MyBss_n Allocated in a section

#pragma section
int __near ni_2;        //.bss Allocated to the section

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • 本文是否實用?