跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

E0551302 Error Message (RL78 CC-RL)

Latest Updated:12/05/2016

Question:

I’m using the RL78 CC-RL compiler. Error message E0551302 appears when I try to describe the assembler directives in the SADDR area of the RAM as the example below. Is there any workaround? “E0551302 : Specified address is out of saddr area.”
 
<Example>
MOVW 0xFE20, AX

Answer:

The value specified for the operand is outside of the saddr area.
Specify the address which is inside of the saddr area.
 
<Example>
MOVW 0xFFE20, AX
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • 本文是否實用?