跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Do I have to connect to a network to use a floating license?

Last Updated:05/17/2017

Question:

Do I have to connect to a network to use a floating license?

Answer:

Yes, you must. You cannot acquire the license without connecting to a network (the server PC).

However, you can hold the license over a certain period, and use it over that period in a state disconnected from the network environment after acquiring it.

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 本文是否實用?