跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Additional feature of the Professional edition with a license for the Standard edition

Last Updated:05/17/2017

Question:

What will happen if I attempt to use an additional feature of the Professional edition with a license for the Standard edition?

Answer:

An error message or warning will be output at the time of building.

[Example: CC-RH]

The following compilation error will occur if you attempt to use MISRA rule checking by specifying the –Xmisra option. 
E0511178: “-Xmisra2004/2012” option has no effect with this license. The following compilation error will occur if you attempt to include code for detecting stack smashing by specifying the –Xstack_protector option.
E0511178: “-Xstack_protector/-Xstack_protector_all” option has no effect with this license. If you attempt to use the facilities for detecting stack smashing in the form of a language extension (#pragma directive), the following warning will be output and the language extension will be ignored.
W0523009: This #pragma has no effect.

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 本文是否實用?