跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Would problems occur if the input V were exceed to maximum rate?

Latest Updated:08/01/2007

Question:

If the input voltage were to exceed the absolute maximum rating even momentarily, would not any problems occur?

Answer:

Reliability cannot be guaranteed and the device may be destroyed.
Renesas Electronics designs devices including their withstanding voltage, in order to guarantee input voltage ratings, including long-term reliability, but if the input voltage may exceed the absolute maximum rating, be sure to provide an external protection circuit.
Suitable Products