跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Why is there a waiting time of 1 bit before TE bit or RE bit of SCR is set to 1?

Latest Updated:03/26/2009

Question:

When initializing the SCI, a waiting time of at least 1 bit is provided before TE bit or RE bit of Serial Control Register (SCR) is set to 1. What is the reason?

Answer:

The waiting period of 1 bit is the minimum time in order to initialize the internal state of SCI. If you don't wait the time before sending the data, erroneous data may be sent.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902