Why is there a delay between vector read and transfer information read?
Latest Updated:03/23/2009
Question:
On the H8S/2xxx DTC operation, there is s one-cycle delay between the vector read and transfer information read. Why?
Answer:
Address calculation
Suitable Products
H8S/2668 |
H8S/2655 |
H8S/2643 |
H8S/2633 |
H8S/2628 |
H8S/2615 |
H8S/2612 |
H8S/2437 |
H8S/2368 |
H8S/2398, 2357 |
H8S/2355 |
H8S/2350 |
H8S/2345 |
H8S/2282, 2280 |
H8S/2276 |
H8S/2258, 2239, 2238, 2237, 2227 |
H8S/2245 |
H8S/2215 |
H8S/2214 |
H8S/2199R |
H8S/2194 |
H8S/2172 |
H8S/2168 |
H8S/2158 |
H8S/2140B |
H8S/2114R |
H8S/2111B |
H8S/2110B |