跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Where would I find the comparison information when replacing MCUs?

Latest Updated:03/13/2008

Question:

(MCU Comparison, Migration)  I would like comparison information for reference when replacing MCUs. Where would I be able to find this? [2008/03/13]

Answer:

Click the Group of any MCU you would like to compare.

Click:
3822A 3823 3826A 38C2A 38D2 38D5 7560A 3803 3803H 3850H 3850A 3851 3858 3886
7540 7542 7542TV 7546 7547 7548 7549 Other Groups

Data on differences between products in the same Group and between Groups is available in PDF files below "Overview" on the above pages or from "Application Notes" in the left side menu. (#105449)

Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7546
7547
7548
7549