跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What would happen if I set ILVL0-ILVL2 to ""7"" ?

Latest Updated:10/10/2006

Question:

When the interrupt priority level select bits (ILVL0-ILVL2) are "0"(disable the interrupt) and interrupt request bit (IR) is "1" (interrupt request), what would happen if I set ILVL0-ILVL2 to "7" (interrupt: served, the interrupt priority level: the highest priority)?
Will the interrupt routine be accepted?

Answer:

The interrupt routine will be accepted if the interrupt flag(I flag) is "1"(served), but the operation timing is affected by the non-maskable interrupt or other interrupts which make ILVL0-ILVL2 "7" (in process or not etc.).
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC