跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the initial value of EEPROM after the shipment?

Latest Updated:03/26/2009

Question:

What is the initial value of EEPROM after the shipment?

Answer:

All values are set to H'FF.
Suitable Products
H8/300H Tiny
H8/36109
H8/36077, H8/36079
H8/36049
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902