跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is THE valid range in the input threshold control register VLTi?

Latest Updated:04/02/2012

Question:

What is the valid range for the input level switching function in the input threshold control register (VLTi)?

Answer:

The input level switching function is valid only when reading the pin input level and the input level is decided depending on the voltage level of the input threshold value selected in the input threshold control register. Verify items of VIH and VIL CMOS input in the electrical characteristics for input “H” voltage and “L” voltage.
Also verify items of VIH and VIL, other than CMOS input in the electrical characteristics for input “H” voltage and “L” voltage when pins are set as peripheral function pins. Furthermore, peripheral function pins include hysteresis characteristics, so verify VT+-VT- in the electrical characteristics.
Suitable Products
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/32M
R8C/33M
R8C/34M
R8C/35M
R8C/36M
R8C/38M
R8C/3GM
R8C/3JM
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
R8C/L35M
R8C/L36M
R8C/L38M
R8C/L3AM
R8C/LA3A
R8C/LA5A
R8C/LA6A
R8C/LA8A
R8C/LAPS