跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What happens to the A/D conversion value if the analog input pin is open?

Latest Updated:03/01/2005

Question:

(A/D Converter)  What happens to the A/D conversion value if the analog input pin is open due to disconnection of the external resistor or other wiring ? [2005/03/01]

Answer:

If the analog input pin is open, the A/D conversion result will be indeterminate. (#104833)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549