跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What happens if data write overlaps with underflow when using R1H or R2H ?

Latest Updated:01/16/2006

Question:

(Timer)   There is a note stating, "When writing data to each reload register R1H or R2H of timer 1 or timer 2 while timer 1 or timer 2 is operating, avoid a timing when timer 1 or timer 2 underflows." What happens if the data write overlaps with underflow? [2006/01/16]

Answer:

Timer as well as reload register values may be undefined. (#105583)
Suitable Products
4508
4509