跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What happen if program counter specifies area of ROM/ RAM due to noise?

Latest Updated:03/01/2005

Question:

(CPU)  What will happen if the program counter specifies an unassigned area of the ROM or RAM due to noise, etc.? [2005/03/01]

Answer:

MCU operation becomes unstable because the fetched ROM data is undefined. (#104744)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549