跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What happen if data is executed without stopping prescaler and timer?

Latest Updated:03/04/2005

Question:

(Timer)   What will happen if the data read instruction is executed without stopping the counter for the programmable prescaler and timer? [2005/03/04]

Answer:

The counter value may not be read correctly. (#105065)
Suitable Products
4508
4509
4559
455A
4571