跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What are the specific frequencies of φSOURCE in timer block diagram?

Latest Updated:06/06/2007

Question:

(Timer)  What are the specific frequencies of the φSOURCE in the timer block diagram? [2007/06/06]

Answer:

Medium and high-speed modes:
     φSOURCE = f(Xin)
Low-speed mode:
     φSOURCE = f(Xcin)
On-chip oscillator mode:
     φSOURCE = on-chip oscillating frequency divided by 4

(#106721)

Suitable Products
38D2
38D5