跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What's the difference between H8/3644 standard mask and R mask?

Latest Updated:01/27/2009

Question:

What are the differences between the H8/3644 standard mask and R mask devices ?

Answer:

The original version of the H8/3644 was designed to operate at 10 MHz but due to demand, the R version was introduced providing operation up to 16 MHz. The R version has also been optimised to improve EMC performance.

Suitable Products
H8/300L
  • 本文是否實用?